Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objFeatures As SolidEdgePart.Features
Dim objBodyFt As SolidEdgePart.BodyFeature
Dim objFaces As Object
Const TESTFILE = "T:\vbtests\testcases\BodyFtr.x_t"
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Open the TestFile
Set objDoc = objApp.Documents.OpenWithTemplate(TESTFILE, "Normal.par")
' Get the Features collection object
Set objFeatures = objDoc.Models(1).Features
Set objBodyFt = objFeatures.Item(1)
If objBodyFt.Type <> igBodyFeatureObject Then
MsgBox ("Not a BodyFeature object")
End If
' Get the Faces using FacesByRay property
Set objFaces = objBodyFt.FacesByRay(xOrigin:=0, yOrigin:=0.05, ZOrigin:=0.05, Xdir:=1, Ydir:=0, Zdir:=0)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objFeatures = Nothing
Set objBodyFt = Nothing
Set objFaces = Nothing
End Sub