Solid Edge Part Type Library
Type Property
Description
Specifies the type of the object being referenced.
Property type
Read-only property
Syntax
Visual Basic
Public Property Type As FeatureTypeConstants
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objFeatures As SolidEdgePart.Features
    Dim objBodyFt As SolidEdgePart.BodyFeature
    Const TESTFILE = "T:\vbtests\testcases\BodyFtr.x_t"
    Dim cType As FeatureTypeConstants
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.OpenWithTemplate(TESTFILE, "Normal.par")
    ' Get the Features collection object
    Set objFeatures = objDoc.Models(1).Features
    Set objBodyFt = objFeatures.Item(1)
    ' Get the Type property
    cType = objBodyFt.Type
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objFeatures = Nothing
    Set objBodyFt = Nothing
End Sub
See Also

BodyFeature Object  | BodyFeature Members