Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
ClosureType | Sets and returns the closer type for the referenced CloseCorner object. |
CornerGap | Sets or returns the face gap distance of the referenced CloseCorner object. |
CutAngle | Sets or returns the angle of the referenced CloseCorner with V-Shaped treatment. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
OffsetValue | Sets or returns the offset value of the referenced CloseCorner cutout. |
OverlapRatio | Sets or returns the overlap ratio of the referenced CloseCorner object. |
Parent | Returns the parent object for the referenced object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
SquareSize | Sets or returns the square size of the referenced CloseCorner with square cutout treatment. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
TreatmentDiameter | Sets or returns the diameter of the circular bend relief of the referenced CloseCorner object. |
TreatmentType | Sets and returns the type of treatment for the referenced object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |