Solid Edge Part Type Library : ConstructionModel Object |
ActivateBody | |
GetFacesByAreaOfBody | |
GetFaultsOfBody | |
GetShorterEdgesOfBody | |
GetSliverFacesOfBody | |
GetSmallFacesOfBody | |
GetSpikeFacesOfBody | |
HealAndOptimizeBody | |
SaveBody | Saves the body of this model to the specified document in the specified format |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Body | Returns the Body object for the referenced object. |
BodyName | |
DeleteBlends | Represents a collection of delete blend objects. |
DeleteFaces | Represents a collection of delete face objects. |
DeleteHoles | Represents a collection of delete hole objects. |
DeleteRegions | Represents a collection of Delete Region features |
ExtendSurfaces | Returns the ExtendSurfaces collection. |
FaceMoves | |
FaceOffsets | |
FaceRotates | |
Features | Returns the Features collection object for the referenced Model. |
Intersects | |
IntersectSurfaces | |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsBodyActive | |
IsFacetBody | |
ModelRecomputeEvents | Returns the ModelRecomputeEvents object for the referenced Model object. |
OffsetEdges | Returns the OffsetEdges collection. |
Parent | Returns the parent object for the referenced object. |
PartingSplits | Returns the PartingSplits collection. |
RedefineFaces | |
ResizeBends | Returns the ResizeBends collection. |
ResizeHoles | |
ResizeRounds | |
Rounds | Returns the Rounds collection object for the referenced Model. |
SplitCurves | Returns the SplitCurves collection. |
SplitFaces | Returns the SplitFaces collection. |
Splits | |
Subtracts | |
Threads | Returns the Threads collection object for the referenced Model. |
TrimSurfaces | Returns the TrimSurfaces collection. |
Unions |