Solid Edge Part Type Library
ExternalBoundary Property
Description
Property of copy surface removal of external boundary option.
Property type
Read-write property
Syntax
Visual Basic
Public Property ExternalBoundary As CopySurfaceExternalBoundaryConstants
Remarks
The external boundaries are the boundaries that define the surface to be copied. When you remove them, the copied surface assumes the boundaries of the bounding box. You can only remove external boundaries if there are no stitched surfaces in the select set.
See Also

CopySurface Object  | CopySurface Members