Solid Edge Part Type Library : CrossBrake Object |
Delete | Deletes the referenced object. |
GetStatusEx | Returns the status of the specified object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
Application | Returns the active application object. |
BendAngle | |
BendDirection | |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Faces | |
Lines | |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |