Solid Edge Part Type Library
Add Method
Specifies the Blend features to delete from the associated detailed model.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal BlendsToDelete As Object _
) As DeleteBlend
Parameters
BlendsToDelete
Specifies the Blend features to delete from the associated detailed model.
See Also

DeleteBlends Collection  | DeleteBlends Members