Solid Edge Part Type Library
GetFaces Method
Collapse All
Expand All
Solid Edge Part Type Library
>
DeleteFace Object
: GetFaces Method
Description
Gets the input delete faces of delete face feature.
Syntax
Visual Basic
Public Function GetFaces() As Object
Remarks
This method returns the faces that are bounded by the referenced Edge object (at most two in the two-manifold situation).
See Also
DeleteFace Object
|
DeleteFace Members