Solid Edge Part Type Library
SetFaces Method
Collapse All
Expand All
Solid Edge Part Type Library
>
DeleteFace Object
: SetFaces Method
Specifies the Face objects to be used to produce the DeleteFace object.
Description
Sets the new set of input delete faces to the delete face feature.
Syntax
Visual Basic
Public Sub SetFaces( _ ByVal
Faces
As Object _ )
Parameters
Faces
Specifies the Face objects to be used to produce the DeleteFace object.
See Also
DeleteFace Object
|
DeleteFace Members