A material treatment to an existing face or set of faces.
Object Model
Remarks
It cannot exist independently. Instead, this object modifies existing faces by angling (drafting) them inward or outward. A Draft object can replace a single face or a set of faces. If the Draft object is created from a set of faces, then all replaced material acts as one object. Therefore, operations such as deleting and suppressing, for example, affect all faces that comprise the Draft object.