A cutout with a profile that follows a linear, extruded path.
Object Model
Remarks
The ExtrudedCutout object represents an occurrence of an extruded cutout feature in a Part or Sheet Metal document. An extruded cutout feature is a cutout with a profile that follows a linear, extruded path. Except for the base feature, the profile on which this object is based can be either open or closed. For the base feature, the profile must be closed. When the profile is open, its ends are extended to the solid to form a closed intersection.