Solid Edge Part Type Library
ToPlane Property
Description
Sets and returns the RefPlane object from which a protrusion, hole, or cutout feature terminates.
Property type
Read-write property
Syntax
Visual Basic
Public Property ToPlane As Object
Remarks
Termination occurs at the intersection of the feature object and the reference plane. Face objects are not limited to being planar faces. This property applies only to those feature objects created with the AddFromTo method.
See Also

ExtrudedProtrusion Object  | ExtrudedProtrusion Members