Solid Edge Part Type Library : FlangeFeatureConstants Enumeration |
Member | Value | Description |
---|---|---|
seFlangeBendAndFaceChainRelief | 3 | Corner Relief Extending Over The Chain of Adjacent Faces |
seFlangeBendAndFaceCornerRelief | 2 | Corner Relief Over The Adjacent Bend And Face |
seFlangeBendOnlyCornerRelief | 1 | Corner Relief Restricted To The Adjacent Bend Only |
seFlangeBendOutside | 6 | Flange Placement Option - Bend Outside |
seFlangeBendReliefNone | 9 | The Bend Relief Type - None |
seFlangeBendReliefRound | 8 | The Bend Relief Type - Round |
seFlangeBendReliefSquare | 7 | The Bend Relief Type - Square or Rectangular |
seFlangeCornerReliefNone | 10 | The Corner Relief Type - None |
seFlangeMaterialInside | 4 | Flange Placement Option - Material Inside |
seFlangeMaterialOutside | 5 | Flange Placement Option - Material Outside |