Solid Edge Part Type Library
Flange Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetDimensionsReturns the Dimensions collection object for the referenced object.
Public Method GetMatchFaceThis method retrieves user data for the match face.
Public Method GetProfilesReturns the profiles associated with the referenced feature object.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleReturns the feature style.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetMatchFaceThis method sets data about the match face.
Public Method SetProfilesSets the profiles associated with the referenced feature object.
Public Method SetStyleSets the feature style.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BendAngle
Public Property BendRadiusSets and returns the inside radius of the bend.
Public Property BendReliefDepthSets and returns the depth of the bend relief for the specified object.
Public Property BendReliefTypeSets and returns a constant that specifies the Bend relief type.
Public Property BendReliefWidthSets and returns the width of the bend relief for the specified object.
Public Property ConstructionEdgeReturns the ConstructionEdge object for the referenced Flange object.
Public Property CornerReliefTypeProperty That Specifies The Corner Relief Type To Be Used
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property FlangeMaterialSideSpecifies the flange location.
Public Property HotEdgeReturns the HotEdge object for the referenced Flange object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ModelingModeType
Public Property NameReturns the name of the referenced object.
Public Property NeutralFactorSets and returns the neutral factor applied to the bend.
Public Property OffsetType
Public Property OffsetValueThis read-write Double property sets and returns the offset value for the referenced Flange object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ProfileSets and returns the Profile object used to construct the referenced feature object.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property UseGlobalBendRadiusSpecifies whether or not the global bend radius is to be applied to the referenced object.
Public Property UseGlobalBendReliefDepthSpecifies whether or not the global bend relief depth is to be applied to the referenced object.
Public Property UseGlobalBendReliefWidthSpecifies whether or not the global bend relief depth is to be applied to the referenced object.
Public Property UseGlobalNeutralFactorSpecifies whether or not the global neutral factor is to be applied to the referenced object.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

Flange Object