Solid Edge Part Type Library
Gusset Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method ExactRangeThis method sets the exact range parameters for the referenced object.
Public Method GetStatusExReturns the status of the specified object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DieRadiusSets and returns radius value for the top of the referenced feature.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property DistanceSets and returns the constraint distance for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property FormedRadiusThis read-write Double property sets and returns the formed radius value for gusset feature.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property MaterialSideSets and returns the direction in which material was added to the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property NumberOfOccurrencesReturns the number of occurrences.
Public Property OccurrenceSpacingThis read-write Double property sets and returns the spacing between gusset occurrences in the sheet metal document.
Public Property ParentReturns the parent object for the referenced object.
Public Property PatternTypeSets and returns the pattern to apply to the referenced Gusset object.
Public Property ProfileSets and returns the Profile object used to construct the referenced feature object.
Public Property PunchRadiusSets and returns the radius value at the bottom of the referenced feature.
Public Property RoundingThis read-write Double property specifies whether or not rounding is applied to a gusset feature.
Public Property ShapeThis read-write Double property specifies the shape of the gusset in the sheet metal document.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TaperAngleSets and returns the taper angle for the referenced object.
Public Property ThicknessSideSets and returns the side of the profile on which the thickness of the feature object was added.
Public Property TypeSpecifies the type of the object being referenced.
Public Property WidthReturns the width of the referenced object.
See Also

Gusset Object  | Solid Edge V19 - What's New