Solid Edge Part Type Library
GetIsoclineFaces Method
Description
Used to get Isocline Faces
Syntax
Visual Basic
Public Sub GetIsoclineFaces( _
   ByRef NumberofEntities As Long, _
   ByRef IsolclineFaces() As Object _
) 
Parameters
NumberofEntities
IsolclineFaces
Example
Imports System.Runtime.InteropServices
Public Class IsoclinecurveEdit

    Private Sub Button1_Click(sender As System.Object, e As System.EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application
        Dim objIsoclineCurves As SolidEdgePart.IsoclineCurves
        Dim objIsoclineCurve As SolidEdgePart.IsoclineCurve
        Dim objPartDoc As SolidEdgePart.PartDocument
        Dim objIsoclinePlane As SolidEdgePart.RefPlane
        Dim objEditPlane As SolidEdgePart.RefPlane

        Dim objConstructions As SolidEdgePart.Constructions
        Dim objSurfArray As System.Array
        Dim objEditArray As System.Array = Nothing
        Dim objFaces As SolidEdgeGeometry.Faces
        Dim Name As String

        Dim dIsoclineAngle As Double
        Dim dEditAngle As Double
        Dim IsolclineDirection As SolidEdgePart.IsoclineDirectionConstants
        Dim Exsurface As SolidEdgePart.ExtrudedSurface
        Dim featureType As SolidEdgePart.FeatureTypeConstants
        Dim objType As Type = Nothing

        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If
            'Get reference to active document
            objPartDoc = objApplication.ActiveDocument

            ' Get the construction object
            objConstructions = objPartDoc.Constructions

            ' Get the isoclineCurves as collection object.
            objIsoclineCurves = objConstructions.IsoclineCurves
            Exsurface = objConstructions.ExtrudedSurfaces.Item(1)

            ' Get all the faces of extruded surface
            objFaces = Exsurface.Faces(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)
            objSurfArray = Array.CreateInstance(GetType(System.Object), 4)

            For value = 1 To objFaces.Count()
                objSurfArray(value - 1) = objFaces.Item(value)
            Next

            dIsoclineAngle = 0.7853
            dEditAngle = 0.0349

            ' Get the reference plane
            objIsoclinePlane = objPartDoc.RefPlanes.Item(2)

            ' Creates the isocline curve
            objIsoclineCurve = objIsoclineCurves.Add(1, objSurfArray, objIsoclinePlane, SolidEdgePart.IsoclineDirectionConstants.igIsoclineRight, dIsoclineAngle)

            Name = objIsoclineCurve.Name()
            featureType = objIsoclineCurve.Type

            ' Edit the isocline Curve.

            ' Change  the direction to igisoclineRight
            objIsoclineCurve.IsoclineDirection = SolidEdgePart.IsoclineDirectionConstants.igIsoclineRight

            ' Getting the current direction
            IsolclineDirection = objIsoclineCurve.IsoclineDirection

            ' Get the current plane
            objEditPlane = objIsoclineCurve.IsoclinePlane

            ' Set the plane 
            objIsoclineCurve.IsoclinePlane = objIsoclinePlane

            'Set the angle
            objIsoclineCurve.IsoclineAngle = dEditAngle

            ' Get the isocline angle
            dIsoclineAngle = objIsoclineCurve.IsoclineAngle

            ' Set the new faces
            objIsoclineCurve.SetIsoclineFaces(1, objEditArray)

            ' get the current faces
            objIsoclineCurve.GetIsoclineFaces(1, objEditArray)

            Call objIsoclineCurve.Delete()

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class
See Also

IsoclineCurve Object  | IsoclineCurve Members