Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EndParentEdge | Sets and returns the Edge object from which the last keypoint in the curve was derived for the referenced KeypointCurve object. |
EndpointEndCondition | Sets and returns the end condition of the last keypoint in the curve for the referenced KeypointCurve object. |
EndpointMagnitude | Sets and returns the direction and degree of influence of the EndpointEdge on the curvature of the curve at the endpoint. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | Returns the modeling mode of the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
ShowCurvatureComb | Toggles the display of curvature combs for the referenced object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
StartParentEdge | Sets and returns the Edge object from which the first keypoint in the curve was derived for the referenced KeypointCurve object. |
StartpointEndCondition | Sets and returns the end condition of the first keypoint in the curve for the referenced KeypointCurve object. |
StartpointMagnitude | Sets and returns the direction and degree of influence of the StartpointEdge on the curvature of the curve at the startpoint. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |