Solid Edge Part Type Library
Tail Property
Collapse All
Expand All
Solid Edge Part Type Library
>
LabelWeldData Object
: Tail Property
Description
Specifies whether the less than symbol appears at the end of the breaklline.
Property type
Read-write property
Syntax
Visual Basic
Public Property Tail As
DimWeldTailTypeConstants
Remarks
If this symbol is included, the Tail property also specifies if the symbol is open or closed.
See Also
LabelWeldData Object
|
LabelWeldData Members