Solid Edge Part Type Library
LabelWeld Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetStatusExReturns the status of the specified object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
See Also

LabelWeld Object