Solid Edge Part Type Library > Load Object : GetLoadOptions Method |
Visual Basic |
---|
Public Sub GetLoadOptions( _ ByRef eLoadType As FEALoadTypeEnum_Auto, _ ByRef dLoadValue As Double, _ ByRef dLoadValueAngAcceln As Double, _ ByRef eLoadDir As LoadSymbDirOptsEnum_Auto, _ ByRef x As Double, _ ByRef y As Double, _ ByRef z As Double, _ ByRef xx As Double, _ ByRef yy As Double, _ ByRef zz As Double, _ ByRef colorLoadSymbol As ULong, _ ByRef colorLoadSymbolAngAcc As ULong, _ ByRef dSpacingFactor As Double, _ ByRef dSizeFactor As Double, _ ByRef dSteeringWheelLen As Double, _ ByRef dwLoadProps As ULong, _ ByRef dLoadSymSpacing As Double, _ ByRef dLoadSymSize As Double _ ) |
Value | Description |
---|---|
eLoadTypeBearing_Auto | |
eLoadTypeCentrifugal_Auto | |
eLoadTypeEnforcedDisplacement_Auto | |
eLoadTypeEnforcedRotation_Auto | |
eLoadTypeForce_Auto | |
eLoadTypeGravity_Auto | |
eLoadTypeMoment_Auto | |
eLoadTypeNone_Auto | |
eLoadTypePressure_Auto | |
eLoadTypeSSHTConvection_Auto | |
eLoadTypeSSHTHeatflux_Auto | |
eLoadTypeSSHTHeatGeneration_Auto | |
eLoadTypeSSHTRadiation_Auto | |
eLoadTypeSSHTTemperature_Auto | |
eLoadTypeTemperature_Auto | |
eLoadTypeTorque_Auto |
Value | Description |
---|---|
eLoadDirAboutAxis_Auto | |
eLoadDirAlongVec_Auto | |
eLoadDirCentrifugal_Auto | |
eLoadDirComponents_Auto | |
eLoadDirDefault_Auto | |
eLoadDirForCnstr_Auto | |
eLoadDirGravity_Auto | |
eLoadDirHeatFlux_Auto | |
eLoadDirNormalToFace_Auto | |
eLoadDirTorque_Auto |