Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Depth | Sets and returns the distance that the referenced object extends or removes material from a solid. |
DepthDirection | Sets and returns the direction of the referenced Louver object. |
DieRadius | Sets and returns radius value for the top of the referenced feature. |
DimensionType | Sets and returns the type of dimension for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EndType | Sets and returns the type of end treatment for the referenced Louver object. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
Height | Returns the height of the referenced object. |
HeightDirection | Sets and returns the direction in which the height of the referenced Louver object is to project. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
RoundType | Returns the type of radii used in the referenced object for a specified edge. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |