Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objCPScaled As SolidEdgePart.Model
Dim objCPMirrored As SolidEdgePart.Model
Dim objCPFlatten As SolidEdgePart.Model
Const TESTFILE = "T:\vbtests\testcases\CapEndRH.psm"
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' creating a scaled copy of the test case file
Set objCPScaled = objDoc.Models.AddCopiedPart(Filename:=TESTFILE, Xscale:=0.75, Yscale:=0.5, Zscale:=0.25)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objCPScaled = Nothing
Set objCPMirrored = Nothing
Set objCPFlatten = Nothing
End Sub