Solid Edge Part Type Library
BottomCap Property
Collapse All
Expand All
Solid Edge Part Type Library
>
NormalCutout Object
: BottomCap Property
Description
Returns the bottom face of a feature object.
Property type
Read-only property
Syntax
Visual Basic
Public Property BottomCap As Object
Remarks
The BottomCap is the face opposite from the face that is in the same plane as the profile that was used to create the feature. This property generates an automation error if no bottom cap exists for the feature.
See Also
NormalCutout Object
|
NormalCutout Members