Solid Edge Part Type Library
TopCap Property
Description
Returns the top face of the referenced feature object.
Property type
Read-only property
Syntax
Visual Basic
Public Property TopCap As Object
Remarks
The TopCap is the face in the same plane as the profile that is used to create the feature. This property generates an automation error if no top cap exists for the feature.
See Also

NormalCutout Object  | NormalCutout Members