Solid Edge Part Type Library
NormalToFaceCutout Object
Members
Collapse All
Expand All
Solid Edge Part Type Library
: NormalToFaceCutout Object
Description
A cutout with closed curves that follows a path normal to the faces on which the curves lie.
Object Model
Remarks
The NormalToFaceCutout object represents an occurrence of a cutout feature that is normal to a face in a Part or Sheet Metal document.
See Also
NormalToFaceCutout Members