Solid Edge Part Type Library > PartDocument Object : GetLiveRules Method |
Visual Basic |
---|
Public Sub GetLiveRules( _ ByVal LiveRule As LiveRulesConstants, _ ByRef bMaintain As Boolean _ ) |
Value | Description |
---|---|
igConcentricLiveRule | Maintain concentric relations |
igCoplanarAxesAboutXLiveRule | |
igCoplanarAxesAboutYLiveRule | |
igCoplanarAxesAboutZLiveRule | |
igCoplanarAxesLiveRule | Maintain coplanar Axes. Always on for live rules in an FOP and cannot be turned off. |
igCoplanarLiveRule | Maintain coplanar relations |
igMaintainRadiusLiveRule | Maintain same radius if possible |
igOrthoLockingLiveRule | Maintain orthogonal to base if possible |
igParallelLiveRule | Maintain parallel relations |
igPerpendicularLiveRule | Maintain perpendicular relations |
igSymmetricLiveRule | Maintain symmetric relations |
igSymmetricXYLiveRule | Maintain symmetric relations based on XY plane |
igSymmetricYZLiveRule | Maintain symmetric relations based on YZ plane |
igSymmetricZXLiveRule | Maintain symmetric relations based on ZX plane |
igTangentEdgeLiveRule | Maintain connected tangent relations |
igTangentTouchingLiveRule | Maintain touching tangent relations |
igThicknessChainLiveRule |