Solid Edge Part Type Library
Plot Object Members
Overview 
Public Methods
Public Method GetMaxNodeOnBodyGets the node with maximum value on the given body.
Public Method GetMaxNodeOnSurfaceGets the node with maximum value on the given surface.
Public Method GetMinMaxValuesGet minimun and maximum stress/displacement values.
Public Method GetMinNodeOnBodyGets the node with minimum value on the given body.
Public Method GetMinNodeOnSurfaceGets the node with minimum value on the given surface.
Public Method GetNearestNodeReturns the data on the node nearest to xyz. In the case of a tie, the first node found should be used.
Public Method GetNodesOnFaceReturns all the Nodes on a given face as an array or list
Public Method GetPlotTypeGet plot object type.
Public Method GetXYZLocationsOfMaxValueGet maximum values at X, Y and Z locations.
Public Method GetXYZLocationsOfMinValueGet minimum values at X, Y and Z locations.
Public Method SavePlotAsImageSave plot display as an image to given location.
Public Method SavePlotAsMovieSave plot animation as a movie to given location.
See Also

Plot Object  | Solid Edge ST3 - What's New