Solid Edge Part Type Library
FeatureCommandType Property
Collapse All
Expand All
Solid Edge Part Type Library
>
Profiles Collection
: FeatureCommandType Property
Description
Sets and returns the type of feature for which the profile is being created.
Property type
Read-write property
Syntax
Visual Basic
Public Property FeatureCommandType As Long
Remarks
You can use this value when adding a profile to determine whether or not the profile is valid for the specified feature type.
See Also
Profiles Collection
|
Profiles Members