Solid Edge Part Type Library > RedefineFace Object : SetEdgeTangencyTypes Method |
Visual Basic |
---|
Public Sub SetEdgeTangencyTypes( _ ByVal NumberOfEdgesAndTypes As Long, _ ByRef BoundaryEdgesArray() As Object, _ ByRef TangencyTypeArray() As RedefineFaceTangencyType _ ) |
Value | Description |
---|---|
igRedefineFaceCurvatureContinuous | |
igRedefineFaceNatural | |
igRedefineFaceNormalToPlane | |
igRedefineFaceTangentContinuous |
All the edges need not be input to it. Only the edges for which tangency types is to be changed can be sent.
NOTE: We must roll to previous feature before we get/set tangency types for edges. This is because the tangency is set on edges which are present before creating redefine feature. Also, roll to current feature after setting tangency types to see the changes.