The RefAxis object is a linear object that defines the axis of cylindrical-based features: revolved protrusions, revolved cutouts, and holes. For revolved features, a RefAxis object is a parent of the feature and is provided as input when creating the feature. For Hole features, a RefAxis object is a resulting child of the feature and can be referenced when creating other revolved features.