Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile As SolidEdgePart.Profile
Dim objLine As SolidEdgeFrameworkSupport.Line2d
Dim objRefAxis As SolidEdgePart.RefAxis
Dim objRefAxis1 As SolidEdgePart.RefAxis
Dim objAttributeSets As Object
Dim lngStatus As Long
Dim bIsAttribPresent As Boolean
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
On Error GoTo 0
'Create a Profile object
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(3))
'Create a Line Object
Set objLine = objProfile.Lines2d.AddBy2Points(x1:=0, y1:=-0.05, x2:=0, y2:=0.05)
' Check the validation criteria of the profile
lngStatus = objProfile.End(ValidationCriteria:=igProfileSingle)
If (lngStatus <> 0) Then
MsgBox "Profile for the reference axis is not open"
End If
' Create a reference axis using the line.
Set objRefAxis = objProfile.SetAxisOfRevolution(lineforaxis:=objLine)
'Create a RefAxis object
Set objRefAxis1 = objDoc.RefAxes(1)
'Set an Attibute Set "MyAttrib""
Set objAttributeSets = objRefAxis.AttributeSets.Add("MyAttrib Set")
'Check the Attribute Set presence "MyAttrib Set"
bIsAttribPresent = objRefAxis.IsAttributeSetPresent("MyAttrib Set")
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile = Nothing
Set objLine = Nothing
Set objRefAxis = Nothing
Set objRefAxis1 = Nothing
Set objAttributeSets = Nothing
End Sub