Solid Edge Part Type Library
RefPlane Object
Members 
Description
A planar object that provides a flat surface on which to create a profile within profile-based features.
Object Model
RefPlane ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle Object
Remarks
Every profile-based feature has a reference plane associated with it. Interactively, the reference plane can be explicitly created or implied, although when a reference plane is implied, an explicit one is created internally. Through automation, all reference planes are created explicitly through the RefPlanes collection object.
See Also

RefPlane Members