Solid Edge Part Type Library
Add Method
Specifies the faces you want to replace.
Specifies the faces, surfaces, or plane that will replace the part face. You can specify contiguous or noncontiguous faces.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal FacesToReplace As Object, _
   ByVal ReplaceSurface As Object _
) As ReplaceFace
Parameters
FacesToReplace
Specifies the faces you want to replace.
ReplaceSurface
Specifies the faces, surfaces, or plane that will replace the part face. You can specify contiguous or noncontiguous faces.
See Also

ReplaceFaces Collection  | ReplaceFaces Members