Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objModel As SolidEdgePart.Model
Dim objEdges As Object
Dim objEdgeArray(1 To 1) As SolidEdgeGeometry.Edge
Dim objRounds As SolidEdgePart.Rounds
Dim objRound As SolidEdgePart.Round
Dim dblRadiusArray(1 To 1) As Double
Dim lngStatus As Long
Dim bShowDims As Boolean
Const TESTFILE = "T:\vbtests\testcases\cube.par"
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
Call objDoc.Close
' opening the test case file
Set objDoc = objApp.Documents.Open(TESTFILE)
Set objModel = objDoc.Models(1)
Set objRounds = objModel.Rounds
' *** creating a simple round on a single edge
' defining the radius for rounding an edge
Set objEdges = objModel.ExtrudedProtrusions(1).Edges(edgetype:=igQueryAll)
Set objEdgeArray(1) = objEdges(1)
dblRadiusArray(1) = 0.005
' creating the round feature
Set objRound = objRounds.Add(NumberOfEdgeSets:=1, EdgeSetArray:=objEdgeArray, _
RadiusArray:=dblRadiusArray)
If objRound.Status <> igFeatureOK Then
MsgBox "Round feature failed"
End If
'Get the present status of ShowDimensions
bShowDims = objRound.ShowDimensions
'Turn on the dimensions
objRound.ShowDimensions = Not bShowDims
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objModel = Nothing
Set objEdges = Nothing
Set objEdgeArray(1) = Nothing
Set objRounds = Nothing
Set objRound = Nothing
End Sub