Solid Edge Part Type Library
Reorder Method
Specifies the feature object for which the referenced feature object is to be inserted in front of or behind.
Specifies if the active feature object is to be placed before or after the target object. If this argument is True, the active feature object is inserted before the target object. If this argument is False, the feature object is placed after the target object.
Description
Inserts the referenced object in front of or behind another feature.
Syntax
Visual Basic
Public Sub Reorder( _
   ByVal TargetFeature As Object, _
   ByVal InsertBefore As Boolean _
) 
Parameters
TargetFeature
Specifies the feature object for which the referenced feature object is to be inserted in front of or behind.
InsertBefore
Specifies if the active feature object is to be placed before or after the target object. If this argument is True, the active feature object is inserted before the target object. If this argument is False, the feature object is placed after the target object.
See Also

SplitCurve Object  | SplitCurve Members