Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BeadMaterialLength | Sets and returns the bead material length for the referenced StitchWeld object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EndOffset | Sets and returns the length of material to remove from the end of the weld bead for the referenced StitchWeld object. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
GapLength | Sets and returns the gap length between solid portions of the bead for the referenced StitchWeld object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
StartOffset | Sets and returns the length of material to remove from the start of the weld bead for the referenced StitchWeld object. |
Status | Returns the status of the specified object. |
StitchWeldAnnotationFormat | Sets and returns the annotation format for the referenced StitchWeld object. |
StitchWeldType | Sets and returns the stitch weld type for the referenced StitchWeld object. |
Suppress | Temporarily suppresses the referenced object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |