Solid Edge Part Type Library : StudyOwner Collection |
AddStudy | Create a new study. |
AddThermalStudy | Create a new Heat Transfer study. |
EditStudyGeom | Edit FEA Study Geometry. |
GetActiveStudy | Get handle to currently active study. |
GetNASTRANScratchDirectoryLocation | Get the location of NASTRAN scratch directory. |
GetSettingsList | Get various settings options from a study owner. |
Item | Get Study From Study Owner. |
SetActiveSetting | Set various settings options on a study owner. |
SetAsmDefaultMaterial | |
SetNASTRANScratchDirectoryLocation | Set the location of NASTRAN scratch directory. |
SetStudyActive | Set a specific study as active. Provide study name as input. |
Application | Returns the active application object. |
Count | Returns the number of objects in the referenced collection. |
Parent | Returns the parent object for the referenced object. |