Represents an occurrence of a Thinwall feature in a Part document.
Object Model
Remarks
A Thinwall is a solid feature that is constructed by clearing a volume from a part, leaving a solid shell. Any features that are placed on the Thinwall object at the time that the Thinwall object is created automatically inherit the common thickness of the part. A new Thinwall object cannot be created for features that are added to a part after the creation of the initial Thinwall object. If a feature is reordered to occur before the Thinwall operation was performed, it will be included in the Thinwall operation.