Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile(1 To 2) As SolidEdgePart.Profile
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
Dim objModel As SolidEdgePart.Model
Dim objProf As SolidEdgePart.Profile
Dim objProfileCollection As SolidEdgePart.Profiles
Dim objProfArr(1 To 3) As SolidEdgePart.Profile
Dim objHole As SolidEdgePart.Hole
Dim objHolData As SolidEdgePart.HoleData
Dim objUDPat1 As SolidEdgePart.UserDefinedPattern
Dim objExtProt1 As SolidEdgePart.ExtrudedProtrusion
Dim objExtProt2 As SolidEdgePart.ExtrudedProtrusion
Dim objExtProfile As SolidEdgePart.Profile
Dim lngStatus As Long
Dim i As Integer
Dim vRng As Variant
Dim x1 As Double, y1 As Double, z1 As Double, x2 As Double, y2 As Double, z2 As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Draw the Base Profile
Set objProfile(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(3))
Set objLines = objProfile(1).Lines2d
Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.08, y2:=0)
Call objLines.AddBy2Points(x1:=0.08, y1:=0, x2:=0.08, y2:=0.06)
Call objLines.AddBy2Points(x1:=0.08, y1:=0.06, x2:=0.064, y2:=0.06)
Call objLines.AddBy2Points(x1:=0.064, y1:=0.06, x2:=0.064, y2:=0.02)
Call objLines.AddBy2Points(x1:=0.064, y1:=0.02, x2:=0.048, y2:=0.02)
Call objLines.AddBy2Points(x1:=0.048, y1:=0.02, x2:=0.048, y2:=0.06)
Call objLines.AddBy2Points(x1:=0.048, y1:=0.06, x2:=0.032, y2:=0.06)
Call objLines.AddBy2Points(x1:=0.032, y1:=0.06, x2:=0.032, y2:=0.02)
Call objLines.AddBy2Points(x1:=0.032, y1:=0.02, x2:=0.016, y2:=0.02)
Call objLines.AddBy2Points(x1:=0.016, y1:=0.02, x2:=0.016, y2:=0.06)
Call objLines.AddBy2Points(x1:=0.016, y1:=0.06, x2:=0, y2:=0.06)
Call objLines.AddBy2Points(x1:=0, y1:=0.06, x2:=0, y2:=0)
' Define Relations among the Line objects to make the Profile closed
Set objRelns = objProfile(1).Relations2d
Call objRelns.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(5), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(5), Index1:=igLineEnd, Object2:=objLines(6), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(6), Index1:=igLineEnd, Object2:=objLines(7), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(7), Index1:=igLineEnd, Object2:=objLines(8), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(8), Index1:=igLineEnd, Object2:=objLines(9), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(9), Index1:=igLineEnd, Object2:=objLines(10), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(10), Index1:=igLineEnd, Object2:=objLines(11), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(11), Index1:=igLineEnd, Object2:=objLines(12), Index2:=igLineStart)
Call objRelns.AddKeypoint(Object1:=objLines(12), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
' Check for the Profile Validity
lngStatus = objProfile(1).End(ValidationCriteria:=igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Profile not closed")
End If
'Create the Base Extruded Protrusion Feature
Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
profileArray:=objProfile, _
profileplaneSide:=igRight, _
ExtrusionDistance:=0.05)
objProfile(1).Visible = False
' Check the Status of the Base Feature
If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
MsgBox ("Error in the Creation of Base Protrusion Feature object")
End If
Set objExtProt1 = objModel.ExtrudedProtrusions(1)
'*** Create another feature
Set objExtProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(3))
Call objExtProfile.Circles2d.AddByCenterRadius(x:=0.04, y:=0.01, Radius:=0.0075)
lngStatus = objExtProfile.End(ValidationCriteria:=igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Profile not closed")
End If
Set objExtProt2 = objModel.ExtrudedProtrusions.AddFinite(Profile:=objExtProfile, _
ProfileSide:=igRight, profileplaneSide:=igLeft, Depth:=0.025)
objExtProfile.Visible = False
'*******Create an UDP with RegularHoles (simpleHoles)
' Create a new profile to use for the feature.
Set objProf = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
' Define the location for three holes.
Call objProf.Holes2d.Add(xCenter:=-0.02, yCenter:=0.03)
Call objProf.Holes2d.Add(xCenter:=-0.01, yCenter:=0.043)
Call objProf.Holes2d.Add(xCenter:=-0.01, yCenter:=0.01)
objProf.Visible = False
lngStatus = objProf.End(ValidationCriteria:=igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Invalid Profile")
End If
Set objProfileCollection = objProf.Parent.Profiles
' Load an array with these profiles.
For i = 1 To objProfileCollection.Count
Set objProfArr(i) = objProfileCollection(i)
Next
' Create the HoleDataOjbect to define the hole parameters.
Set objHolData = objDoc.HoleDataCollection.Add(HoleType:=igRegularHole, _
HoleDiameter:=0.01)
' Create a hole feature to serve as the seed feature.
Set objHole = objModel.Holes.AddFinite(Profile:=objProfileCollection(1), _
profileplaneSide:=igRight, _
FiniteDepth:=0.016, _
Data:=objHolData)
If objHole.Status <> igFeatureOK Then
MsgBox ("Error in the Creation of Hole object")
End If
' Create the UDP with the AddByProfiles method
Set objUDPat1 = objModel.UserDefinedPatterns.AddByProfiles(NumberOfProfiles:= _
objProfileCollection.Count, ProfilesArray:=objProfArr, _
SeedFeature:=objHole)
' Check the status of UserDefinedPattern Feature
If objUDPat1.Status <> igFeatureOK Then
MsgBox ("Error in the Creation of UserDefinedPattern with RegularHoles")
End If
'Reorder the UserDefinedPattern ahead of Hole1
Call objUDPat1.Reorder(targetfeature:=objExtProt1, InsertBefore:=False)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile(1) = Nothing
Set objProfile(2) = Nothing
Set objLines = Nothing
Set objRelns = Nothing
Set objModel = Nothing
Set objProf = Nothing
Set objProfileCollection = Nothing
Set objProfArr(1) = Nothing
Set objProfArr(2) = Nothing
Set objProfArr(3) = Nothing
Set objHole = Nothing
Set objHolData = Nothing
Set objUDPat1 = Nothing
Set objExtProt1 = Nothing
Set objExtProt2 = Nothing
Set objExtProfile = Nothing
End Sub