Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
DraftAngle | Specifies the draft angle. |
DraftEnabled | Specifies whether draft is enabled. |
DraftFromOutsideEdges | Specifies how draft angle is measured for the referenced object. |
DraftSide | Specifies the draft side. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
ExtentDepth | Sets and returns the extent depth. |
ExtentSide | Sets and returns the extent side. |
ExtentType | Sets and returns the extent type. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | Returns the modeling mode of the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
RibDepth | Specifies the rib depth. |
RibExtension | Specifies the distance the ribs extend past the exterior boundary. |
RibOffset | Specifies the distance the ribs are offset from the entrance surface. |
RibThickness | Specifies the rib thickness. |
RoundEnabled | Specifies whether rounding is enabled for the referenced object. |
RoundRadius | Specifies the round radius. |
ShowDimensions | Controls the display of dimensions for the feature object. |
SparDepth | Specifies the spar depth. |
SparExtension | Specifies the distance the spars extend past the exterior boundary. |
SparOffset | Specifies the distance the spars are offset from the entrance surface. |
SparThickness | Specifies the spar thickness. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |