Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BottomCaps | Returns the BottomCaps collection for the referenced feature object. |
Depth | Sets and returns the distance that the referenced object extends or removes material from a solid. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
ExtentSide | Sets and returns the reference plane side for the referenced object. |
ExtentType | Sets and returns the extent type for the referenced object. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FromPlane | Sets and returns the RefPlane object from which a protrusion, hole, or cutout feature begins. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
SideFaces | Returns a collection of all the side faces for the referenced feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SystemName | This read-only String property returns the system name for the referenced object. |
TopCaps | Returns the TopCaps collection object for the reference object. |
ToPlane | Sets and returns the RefPlane object from which a protrusion, hole, or cutout feature terminates. |
Type | Specifies the type of the object being referenced. |