Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
ChamferSetbackAngle | Returns the angle of the referenced Chamfer object. |
ChamferSetbackValue1 | Sets and returns the distance for the first setback of the referenced Chamfer object. |
ChamferSetbackValue2 | Sets and returns the distance for the second setack of the referenced Chamfer object. |
ChamferType | Returns a constant that specifies how the referenced Chamfer object is defined. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
GetEdgesByModel | Returns the edges of a part occurrence specified by the input model. |
GetFacesByModel | Returns the faces of a part occurrence specified by the input model. |
GetFacesByModelAndRay | Returns the faces of a part occurrence specified by the input model and a ray. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |