Solid Edge Part Type Library
WeldExtrudedCutout Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetInputModelsReturns the objects that are input to the weldment feature.
Public Method GetProfilesReturns the profiles associated with the referenced feature object.
Public Method GetRangeByModelReturns the range of a part occurrence specified by an input model.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleByModelReturns an object that describes the style of the referenced feature.
Public Method SetProfilesSets the profiles associated with the referenced feature object.
Public Method SetStyleSets the feature style.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DepthSets and returns the distance that the referenced object extends or removes material from a solid.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property ExtentSideSets and returns the reference plane side for the referenced object.
Public Property ExtentTypeSets and returns the extent type for the referenced object.
Public Property FromPlaneSets and returns the RefPlane object from which a protrusion, hole, or cutout feature begins.
Public Property GetBottomCapsByModelReturns a collection of bottom cap faces for the specified model.
Public Property GetEdgesByModelReturns the edges of a part occurrence specified by the input model.
Public Property GetFacesByModelReturns the faces of a part occurrence specified by the input model.
Public Property GetFacesByModelAndRayReturns the faces of a part occurrence specified by the input model and a ray.
Public Property GetSideFacesByModelReturns a collection of side faces of the weldment feature from the specified model.
Public Property GetTopCapsByModelReturns a collection of top cap faces of the weldment feature for the specified model.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ProfileSideSets and returns the side of the profile to which material is added or removed.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property ToPlaneSets and returns the RefPlane object from which a protrusion, hole, or cutout feature terminates.
Public Property TypeSpecifies the type of the object being referenced.
See Also

WeldExtrudedCutout Object