Solid Edge Part Type Library
WeldRound Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetConstantRadiiReturns the number of constant radii and the values of those radii for the specified Round object.
Public Method GetInputModelsReturns the objects that are input to the weldment feature.
Public Method GetRangeByModelReturns the range of a part occurrence specified by an input model.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleByModelReturns an object that describes the style of the referenced feature.
Public Method GetVariableRadiiReturns the number of variable radii and the values of those radii for the specified Round object.
Public Method SetConstantRadiiSets the number of constant radii and the values of those radii for the specified Round object.
Public Method SetStyleSets the feature style.
Public Method SetVariableRadiiSets the number of variable radii and the values of those radii for the specified Round object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgeSetCountReturns the number of edges to which the referenced Round feature applies.
Public Property GetEdgesByModelReturns the edges of a part occurrence specified by the input model.
Public Property GetFacesByModelReturns the faces of a part occurrence specified by the input model.
Public Property GetFacesByModelAndRayReturns the faces of a part occurrence specified by the input model and a ray.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property RadiusTypeReturns the radius type for the referenced object.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
See Also

WeldRound Object