Solid Edge ST7 SDK
Solid Edge V16 SP9 - What's New
Problem Reports
Item Description
PR 1412431 Added DrawingView.IsBroken API to indicate if a view is in the broken state.
PR 1392663 Fixed a problem where a macro failed to create interpart constructions.
PR 1410684 Added DrawingView.IsBroken API to indicate if a view is in the broken state.
PR 1406741 UpdateAll automation api updates only the modified documents when debug registry switch UPDATE_ALLMODIFIED_DOCUMENTS is set to 1.
New APIs
SolidEdgeDraft
See Also