--------------
Legal Notices
--------------
© 2005,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 17.00.01.06
Date: 27-MAY-2005
This release of Solid Edge has been certified to run on the following:
• Windows 2000 Professional® operating system running Service Pack 4.
• Windows XP Professional® operating system running Service Pack 1 or 2.
• Internet Explorer 6.0 or higher
This Update should be installed on top of Solid Edge Version:
17.00.00.65
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 2048185: Fixed an abort in Assembly when unhighlighting a part reference plane.
PR 5163104: Fixed an abort in the placement of adjustable part.
PR 1391409: Fixed a problem where interparts would be broken after in-place activating and doing a save as.
PR 1392991: Fixed a problem where relationships on adjustable parts do not update correctly in Move Part.
PR 1394374: Fixed a problem with Pattern of Parts not updating correctly.
PR 2047821: Fixed a problem with the Assembly Feature pattern stagger option not update correctly
PR 5154834: Fixed a problem where Inter Part Copy fails on an assembly
PR 5162558: Fixed a problem with the "Use distance between faces" option is not being honored.
PR 5162897: Fixed a problem where a component sketch cannot be updated after precision graphics are added.
PR 5163176: Fixed a problem with not coping the style in simplified assembly.
PR 5163711: Fixed a performance problem with File Open with Hide All Components.
PR 5167306: Fixed a problem with an occurrence flag not always being reset properly.
PR 5171422: Fixed a problem so that the view style's antialias settings will function correctly.
PR 5185263: Fixed an abort in the Assemble command in some situations.
PR 1395295: Fixed a problem where assembly has two parts that do not show in draft.
PR 5096135: Added logging code to help in diagnosing save failures that users are experiencing.
=====Part=====
PR 5153637: Fixed a problem where material name was limited to 26 characters.
PR 5167515: Fixed an abort with RMB from DynamicEdit
PR 2048022: Fixed a problem where a message box is going behind the Solid Edge window.
PR 5054338: Fixed a problem with missing letters in a text profile.
PR 5134998: Fixed a problem with assembly file open performance and inactive parts.
PR 5141089: Fixed a problem with converting a 4-edge-corner part into Sheet Metal.
PR 5155492: Fixed a problem where Resize Angle was not working properly with Undo.
PR 5159005: Fixed a problem where undoing a change to midsurface was causing the document to close.
PR 5162587: Fixed an abort in the loft command.
PR 5157321: Fixed a case-specific abort.
PR 5109132: Fixed a problem where an Iges file would not import.
PR 5153252: Fixed an abort in SheetMetal Feature Recognizer.
PR 1388943: Fixed a problem where dynamic edit would not work on angular reference planes
PR 2048356: Mass is correctly compute in assembly when 'Show units' option is off in part file.
PR 2048683: Fixed a problem where the Help button on License Wizard did not work.
PR 5170406: Fixed a problem where dimensions flip and cause feature failures when changing FOP members.
PR 5176830: Fixed a problem where adding a material name with " in it removes all other material names.
PR 2049756: Fixed a problem where the material lists will not drop down on Win2000.
PR 5187470: Fixed a problem where the material table command is not available in D&D.
=====Draft=====
PR 1390262: Fixed a problem where parts list balloon quantity is incorrect when opening a draft file without model file
PR 1395101: Fixed a problem where sub-assemblies are still included in the parts list with 'exclude reference parts' option
PR 2047071: Fixed a problem where you can't drag a center mark in "Draw in View" from one element to another
PR 2048161: Fixed a problem in View of Part where folded views had the wrong hidden and/or tangent edge settings.
PR 5159459: Fixed a problem where hidden edges are exporting to dwg as visible with layer mapping
PR 5159653: Fixed a problem where garbage syntax is written to an ini when the original seacad.ini is copied.
PR 5178744: Fixed a problem where doing a Save As Flat to DXF the translator will not distinguish colors
PR 5179033: Fixed a problem that caused drawing views to fail to update when a model file had been opened using mapped network drive.
=====API=====
PR 5163304: Fixed a problem where text on toolbar buttons added using automation is corrupted.
PR 5153634: Modifications to the MechanicalModeling property set now work correctly through the API.
=====Insight=====
PR 1391901: Fixed a problem where a crash occurs during LCA.
PR 5159362: Fixed a problem where removing access for a doc lib results in no access to other doc libs in that site.
PR 1395400: Fixed a problem where setting action to copy an assembly and all parts in RevMgr was causing a silent abort.
PR 2047208: Fixed a problem where the "Where Used" area is not updated properly in revision manager.
PR 5185087: Fixed a problem where Insight connect did not work with an academic university license.
---
End
---