--------------
Legal Notices
--------------
© 2006,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 17.00.10.02
Date: 03-Mar-2006
This release of Solid Edge has been certified to run on the following:
• Windows 2000 Professional® operating system running Service Pack 4.
• Windows XP Professional® operating system running Service Pack 1 or 2.
• Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version:
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03, 17.00.05.03,
17.00.06.03, 17.00.07.03, 17.00.08.03, or 17.00.09.03
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 1476826: Fixed a problem where relationships are not updating after editing parts.
PR 2062434: Fixed a problem where you can't restore the auto backup file in V17
PR 5384474: Fixed a problem where Printing Reports truncate column titles on Jpn version
PR 1502640: Fixed an abort in FlashFit when hitting Flip after a circular dependency error.
PR 5371628: Fixed an abort when deleting a relationship from ribbon bar while in Assembly using Reduced Input mode.
PR 5407218: Fixed a problem where in the assembly file fails to open.
PR 1499431: Fixed a problem with locating target faces on subassembly parts for traditional relationships.
PR 1501482: Fixed a problem with not being able to select faces when using FlashFit in Edit Definition.
PR 1503322: Fixed a problem where Part modifications are reverting when a display configuration is applied.
PR 2060309: Fixed a problem where you are unable to select parts from view
PR 2062548: Fixed a problem where some assembly files would fail to open.
PR 2063432: Fixed a problem with restoring a backup file to a network location.
PR 5347858: Fixed a problem where Assembly features were not reflected at the toplevel
PR 5353329: Fixed a problem where non-auto dimensions were getting hidden when they should not be.
PR 5373421: Fixed a problem where adding a horizontal alignment in hole 28 causes holes to fail.
PR 2060417: Fixed a problem where a Model does not show up
=====Part=====
PR 1466602: Fixed a problem where a Sheet metal part is not being computed when the material name is changed
PR 1494255: Fixed a problem where SE crashed during flatten sheet metal part
PR 2062575: Fixed a problem where Material table APIs crashed
PR 1471984: Fixed a problem where flat pattern fails when recomputing a V14 part ( regression)
PR 5210070: Fixed a problem where a Flyout toolbar button does not show custom bitmap.
PR 5391641: Fixed a problem when loading Parasolid files using Solid Edge API
=====Draft=====
PR 1493661: Fixed a problem where non-rectangular cropping in V15 becomes uncropped when opened in V16 or later.
PR 5393644: Fixed a problem where the Author Field is getting set back to login name when Auto-save is on.
PR 1494809: Fixed a problem where sketches from an assembly shown in a drawing view disappear on update.
PR 2063758: Fixed a problem that caused some V16 files unable to open in V17 or V18.
=====API=====
PR 2063313: Fixed a problem where custom properties are not accessible using propauto for FOA members
=====Insight=====
PR 5388175: Fixed a problem where Add to Library process is not completing when defining a folder contents
PR 5397191: Fixed a problem where you are unable to Save or use Add to Library for a particular part file that is 135 Mb.
PR 5401669: Fixed a problem where Solid Edge search is crashing the w3wp.exe (SharePoint) process.
---
End
---