--------------
Legal Notices
--------------
© 2005,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 17.00.02.04
Date: 27-Jun-2005
This release of Solid Edge has been certified to run on the following:
• Windows 2000 Professional® operating system running Service Pack 4.
• Windows XP Professional® operating system running Service Pack 1 or 2.
• Internet Explorer 6.0 or higher
This Update should be installed on top of Solid Edge Version:
17.00.00.65, 17.00.01.06
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 5189682: Fixed a problem which addressed display related crashes captured via customer submitted crashlogs.
PR 1391151: XpresRoute relation automation has been enhanced to return Reference elements.
PR 5162897: Fixed a problem where assembly sketches disappear from a drawing view
PR 5167399: Fixed a problem in frames which was causing the frames not to update correctly.
PR 5183278: Fixed a problem with constraints not updating correctly after a replace between FOA members.
PR 1384574: Performance for opening large assemblies in Property Manager has been improved.
PR 1377181: Fixes a problem with Web Publisher not publishing properties for parts in an assembly.
PR 1403241: Fixed a problem in which you could not save the file after creating a CAM constraint.
PR 5162968: Fixes a problem with not being able to place simplified assemblies as simplified.
PR 5203598: Fixed a problem with crashes that could occur following Save As X_T or Reports as captured via crashlogs.
PR 1401263: Fixed a problem where Solid Edge crashes in VS+ after SaveAsImage
PR 5140867: Fixed a problem with subassemblies being incorrectly marked as adjustable.
PR 5161476: Fixed a problem with a display anomaly when using a separate window to place parts.
PR 5180530: Fixed a problem where saving a family member with the "save member as" was leaving extra links.
PR 5212021: Fixed a problem that resolved a performance issue when using graphics card driven advanced.
PR 5190058: Fixed a problem where a copied sketch was not maintaining its relative position after updating the assembly.
Please Note: This fix requires that the parent part be activated in the assembly before making changes.
PR 5203211: Fixed a problem where physical properties was returning different results based on selection method.
Please Note, V17 requires the entire ASM be selected for the correct mass to be calculated.
=====Part=====
PR 5195181: Fixed a problem where insert part copy would allow a cyclic dependency.
PR 1394695: Fixed a problem of not taking plane input for intersection curves api.
PR 1400009: Preventing crash inside math.
PR 1400861: Fixed a problem renaming multi-hole features.
PR 5160913: Fixed a problem where numeric separator is changed after creating a part copy of a UG file.
PR 5183185: Fixed a problem where Up line and down line information in the output file is incorrect
PR 5197656: Fixed a problem that will now reduce memory consumption when working with extremely large part models.
PR 5155310: Fixed a case-specific abort when opening file
PR 1404346: Fixed a problem where Delete Holes by Operator was not working.
PR 5170921: Fixed a problem of disabling the trim surface and split surface buttons.
PR 5201694: Fixed a problem with file save failure after changing bead material.
PR 1398448: Fixed a problem that corrected an out of memory while copy/paste in profile segments.
PR 1406329: Fixed a problem that caused a crash because FOP names exceeded max length
PR 2050161: Fixed a problem where the units of mass moments of inertia cannot not be changed.
PR 5205166: Fixed a problem where License Borrowing will now work when the license file contains comments.
PR 5205636: Fixed a problem where you could not create a part copy of a JT file created in NX.
PR 5205928: Fixed a problem where trim was always trimming only on one side.
PR 5206402: Fixed a problem where Solid Edge now displays a more sensible error message when an out of memory condition occurs during file open.
=====Draft=====
PR 5176538: Fixed a problem where SE aborts when this V12 file is opened.
PR 5180284: Fixed a problem of exporting the given draft file to AutoCAD causing Solid Edge to abort
PR 5184685: Fixed a problem of aborting while exporting the given draft file to AutoCAD
PR 5196160: Fixed a problem where locating a textbox is leading to an abort.
PR 5197668: Fixed a problem that caused Solid Edge to abort in undo after using edge painter.
PR 1395118: Fixed a problem translating drawing views to DWG when the specified config is not found.
PR 1400365: Fixed a problem with hatching translated from a metric draft file
PR 1402891: Fixed a problem where multiple page hole tables drift apart on update.
PR 2048446: Fixed a problem associated with undoing the creation of the first line in the cutting plane environment.
PR 2049002: Fixed a problem where linear group dimensions on detail views start from the locate point
PR 5177125: Fixed a problem where stack angular group dimensions are not getting exported correctly.
PR 5177989: Fixed a problem where the callout text is not getting translated out correctly.
PR 5177992: Fixed a problem of fractional dimension display exporting to AutoCAD as decimal.
PR 5179023: Fixed a problem of hidden layers exporting visible during save as flat
PR 5188329: Fixed a problem where drawing views cannot be created after renaming "Normal" fill style.
PR 1402037: Fixed a problem where Solid Edge (v16, v17) would crash when opening some pre-v16 .DFT files.
PR 5183649: Fixed a problem that caused a crash in sheet setup.
PR 1399602: Fixed a problem where ModelLink.Range3d returned an error.
PR 1403923: Fixed a problem with mirroring groups and centerlines
PR 1406215: Fixes a problem where a parts list isn't displayed after being created.
PR 2049537: Fixed a problem where watermark is garbled in Solid Edge Japanese version.
PR 5195356: Fixed a problem that would cause Draft files to fail to open in V17.
PR 5184516: Fixed a problem where "exclude reference parts" causes sub-assembly's with no visible parts to be excluded from the Draft Parts List.
=====MoldTooling=====
PR 5157786: Fixed a problem getting the correct number of sub-occurrences when queried from sub-occurrences API.
=====API=====
PR 1359270: Fixed a problem where OLE for DM container is not displaying SE Part in the embedded object site.
=====Insight=====
PR 1402916: Fixed a problem where SearchScope.txt entries were case sensitive.
PR 5177093: Fixed a problem where opening an assembly with Free Viewer write locks sub-assemblies.
PR 5185350: Fixed a problem where Insight Assistant fails on Jpn OS when WebParts page has JPN chars
PR 5190493: Fixed a problem where, Options file created by Insight Assistant on localized software won't update.
PR 5164307: Fixed a problem where the "Open in Dashboard" menu will now be shown if the user Right clicks on SharePoint URL in search results.
---
End
---