Solid Edge ST7 SDK
Solid Edge V17 SP4 - What's New
Problem Reports
Item Description
PR 1392663 Fixed a problem where a Macro fails to create interpart constructions
PR 1406741 UpdateAll automation API updates only the modified documents when debug registry switch UPDATE_ALLMODIFIED_DOCUMENTS is set to 1.
PR 1410684 Fixed a problem where an addin could encounter an invalid argument exception when working with the edgebar.
PR 5234060 Fixed a problem where the JAsmHideInDrawing occurrence property being incorrectly set.
PR 1392422 Fixed a problem in automation where inconsistent names are returned by igMouse and DVLines.
PR 1412431 Added DrawingView.IsBroken API to indicate if a view is in the broken state.
PR 1402024 Fixed a problem with FOA status property - propauto.dll.
New APIs
SolidEdgeDraft
See Also