--------------
Legal Notices
--------------
© 2005,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 17.00.07.03
Date: 29-Nov-2005
This release of Solid Edge has been certified to run on the following:
• Windows 2000 Professional® operating system running Service Pack 4.
• Windows XP Professional® operating system running Service Pack 1 or 2.
• Internet Explorer 6.0 or higher
This Update should be installed on top of Solid Edge Version:
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03, 17.00.05.03,
17.00.06.03
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 2055227: Fixed a problem where Solid Edge exits when opening this assembly - Japanese OS Specific.
PR 5344939: Fixed a problem based on crashlog files that should resolve several aborts.
PR 1452562: Fixed a problem where Edgebar was not updated after revising a component
PR 5331276: Fixed a problem with the Registry setting for Place Part/Assemble to be Mate
PR 5332702: Fixed a problem with file save in assembly
PR 5346171: Fixed a problem with incorrect part texture being loaded when opening assemblies
PR 2055627: Fixed a problem that cased an abort when saving an assembly configuration.
PR 1468239: Fixed a problem activating display a configuration of a subassembly
PR 2055667: Fixed a problem where you can not open Sub assembly from Main assembly
PR 2055673: Fixed a problem where Configuration list is not retained when returning to a subassembly
PR 5348651: Fixed a problem where FOA is not behaving correctly when changing members
PR 5349577: Fixed a problem where Assembly features are not showing graphically in the display.
=====Part=====
PR 5345416: Fixed a problem that caused Solid edge abort when closing document or exiting the application.
PR 1447589: Fixed a problem that caused an abort when trying to make changes within property manager
PR 5338890: Fixed a problem with features failing with "Unable to recompute topology tracking information"
PR 1466602: Fixed a problem where Changing material name does not fire off recompute for custom formula
PR 1469431: Fixed a problem with Sketch Relationship Color affecting feature update with Dynamic Edit
PR 5348473: Fixed a problem where Material gages are not being saved.
=====Draft=====
PR 2036389: Fixed a problem where Sketch shifts using "by 2 points" dimension
PR 2047352: Fixed a problem where All elements disappear after panning
PR 1469482: Fixed a problem where hidden holes in mirrored partcopy display visible
=====API=====
PR 1449660: Fixed a problem where the entire part is green when opening parasolid from V8-V14 files that had threads.
PR 5344764: Fixed a problem where Revision Manager Replace API is not working correctly when fixing links to FOA members
=====Insight=====
PR 1466763: Fixed a problem with Insight API - DeleteDocumentsFromServer
PR 5347635: Fixed a problem where Property Manager does not list any FOP Children when in the master file
---
End
---